2024-02-23 4:54 PM
Hello
I am using the following to try and get a notification from an STM32WB Nucleo server to my phone the client but cannot get it to work.
BLE Notifications ---- ST Micro video
I compile and can see the two characteristics on my phone but when I push the button on the board my phone never updates with anything. I have tried ST Toolbox and nRF Connect and neither works.
I have attached my project pdf file from CubeMX. This project was built on a test that does Pairing and Bonding with Pairing required only on certain characteristics from the Product service. After this was working successfully I added the STATUS service (page 18) which is pretty similar to the video.
The difference is the VALVE characteristic has permission set to:
ATTR_PERMISSION_AUTHEN_WRITE = YES
and GATT event set to :
GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP = YES
The second characteristic is the NOTIFICATION which the video is based off of (see page 18 of the pdf).
Can anyone please share some light as to what I might try?
Thank you
Steve
2024-03-15 7:51 AM
Hi,
Had the same issue for a week. In my case the "if" statement was the culprit. It is generated in a way, that it never executes the "Custom_Button_c_Update_Char" function.
In my case the name of the service is "myService" and the name of my characteristic is "Button_c"
Try to modify the generated code in the "custom_app.c" file like so:
/* myService */
void Custom_Button_c_Update_Char(void) /* Property Read */
{
uint8_t updateflag = 0;
/* USER CODE BEGIN Button_c_UC_1*/
Custom_STM_App_Update_Char(CUSTOM_STM_BUTTON_C, (uint8_t *)UpdateCharData);
/* USER CODE END Button_c_UC_1*/
if (updateflag != 0)
{
Custom_STM_App_Update_Char(CUSTOM_STM_BUTTON_C, (uint8_t *)UpdateCharData);
}
/* USER CODE BEGIN Button_c_UC_Last*/
/* USER CODE END Button_c_UC_Last*/
return;
}
This way you avoid code modification everytime you re-generate your code.
Also, I can't seem to find the attachment you mentioned.
2024-04-15 6:27 AM
2024-04-16 3:25 AM
Hi SWenn,
I had the same problem with this video tutorial, so I made some changes and share them below:
** custom_app.c **
1)Add these variables:
/* USER CODE BEGIN PV */
uint8_t notifyStatus = 0;
uint8_t button1Status = 0;
/* USER CODE END PV */
2) Modify the fuction:
/* USER CODE BEGIN PFP */
void myTask(void){
if(button1Status != HAL_GPIO_ReadPin(B1_GPIO_Port, B1_Pin)){
button1Status = HAL_GPIO_ReadPin(B1_GPIO_Port, B1_Pin);
NotifyCharData[0] = button1Status;
Custom_Char2_Send_Notification();
}
UTIL_SEQ_SetTask(1<<CFG_TASK_MY_TASK, CFG_SCH_PRIO_0);
}
/* USER CODE END PFP */
3) Modify the fuction:
/* Functions Definition ------------------------------------------------------*/
void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
/* USER CODE BEGIN CUSTOM_STM_App_Notification_1 */
/* USER CODE END CUSTOM_STM_App_Notification_1 */
switch (pNotification->Custom_Evt_Opcode)
{
/* USER CODE BEGIN CUSTOM_STM_App_Notification_Custom_Evt_Opcode */
/* USER CODE END CUSTOM_STM_App_Notification_Custom_Evt_Opcode */
/* Service_1 */
case CUSTOM_STM_CHAR1_WRITE_EVT:
/* USER CODE BEGIN CUSTOM_STM_CHAR1_WRITE_EVT */
/* USER CODE END CUSTOM_STM_CHAR1_WRITE_EVT */
break;
case CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT:
/* USER CODE BEGIN CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT */
notifyStatus = 1;
/* USER CODE END CUSTOM_STM_CHAR2_NOTIFY_ENABLED_EVT */
break;
case CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT:
/* USER CODE BEGIN CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT */
notifyStatus = 0;
/* USER CODE END CUSTOM_STM_CHAR2_NOTIFY_DISABLED_EVT */
break;
case CUSTOM_STM_NOTIFICATION_COMPLETE_EVT:
/* USER CODE BEGIN CUSTOM_STM_NOTIFICATION_COMPLETE_EVT */
/* USER CODE END CUSTOM_STM_NOTIFICATION_COMPLETE_EVT */
break;
default:
/* USER CODE BEGIN CUSTOM_STM_App_Notification_default */
/* USER CODE END CUSTOM_STM_App_Notification_default */
break;
}
/* USER CODE BEGIN CUSTOM_STM_App_Notification_2 */
/* USER CODE END CUSTOM_STM_App_Notification_2 */
return;
}
4)Modify the fuction:
void Custom_Char2_Send_Notification(void) /* Property Notification */
{
uint8_t updateflag = 0;
/* USER CODE BEGIN Char2_NS_1*/
updateflag = notifyStatus;
/* USER CODE END Char2_NS_1*/
if (updateflag != 0)
{
Custom_STM_App_Update_Char(CUSTOM_STM_CHAR2, (uint8_t *)NotifyCharData);
}
/* USER CODE BEGIN Char2_NS_Last*/
/* USER CODE END Char2_NS_Last*/
return;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.