2022-06-09 9:17 AM
I Have updated the Dongle's fuses to 1.2.0 version. I did a successful test with the example of transparent mode and the monitor RF. Now I'm trying to use it as Server in a p2p example and it doesn't works. To discard, I flash it again with the example of the transparaent mode and I now I can't conect with monitor RF giving me the following pop-up.
Is it that the Dongle is broken? I tryed programming on it the heartrate example and it didn't work.
If I read the fuses it response fine:
2022-06-10 7:19 AM
I solved: I put again the ble stack and it worked. First I put in it an other stack (Zigbee) and then I put it the ble stack again and start working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.