2024-06-19 4:04 PM
The directory:
is empty. There should be an "Include" directory here.
This missing directory means that some of the BLE programs (BLE AT Server) cannot compile.
I was on the P-NUCLEO-WB55.Nucleo platform.
The cproject file refers to:
<state>$PROJ_DIR$/../../../../../../Drivers/CMSIS/Device/ST/STM32WBxx/Include</state>
=====
Related problem:
directory: STM32CubeWB-v1.19.1/Drivers/STM32WBxx_HAL_Driver
also does not have the Inc directory but the cproject file has:
<state>$PROJ_DIR$\..\..\..\..\..\..\Drivers\STM32WBxx_HAL_Driver\Inc</state>
====
Bottom line, none of the BLE examples run with v.1.19.1 for the P-NUCLEO-WB55.Nucleo platform.
Solved! Go to Solution.
2024-06-20 2:57 AM
Hello @SWent.1
I'm not able to reproduce this issue. I think you have the same issue as on this post. If so, please follow the recommendations of the same post.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-20 2:57 AM
Hello @SWent.1
I'm not able to reproduce this issue. I think you have the same issue as on this post. If so, please follow the recommendations of the same post.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-25 4:20 PM
git clone --recursive https://github.com/STMicroelectronics/STM32CubeWB.git
yes, the --recursive was needed and resolves the problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.