2022-09-14 12:30 AM
The hardware is B-L072Z-LRWAN1 kit.
In STM32CubeExpansion_LRWAN_V1.3.1 I can change the Data rate and Tx power.
But after update to STM32CubeExpansion_LRWAN_V2.1.0 I can't change data rate and tx power as I want.
The data rate I change by edit LORAWAN_DEFAULT_DATA_RATE, LORAWAN_ADR_STATE is LORAMAC_HANDLER_ADR_OFF.
static LmHandlerParams_t LmHandlerParams =
{
.ActiveRegion = ACTIVE_REGION,
.DefaultClass = LORAWAN_DEFAULT_CLASS,
.AdrEnable = LORAWAN_ADR_STATE,
.TxDatarate = LORAWAN_DEFAULT_DATA_RATE,
.PingPeriodicity = LORAWAN_DEFAULT_PING_SLOT_PERIODICITY
};
#define LORAWAN_DEFAULT_DATA_RATE DR_5
#define LORAWAN_ADR_STATE LORAMAC_HANDLER_ADR_OFF
But when I change LORAWAN_DEFAULT_DATA_RATE only IN865, RU864, EU868, KR920 take effect, AS923 and AU915 data rate is DR_2 (SF10), US915 the data rate is fixed DR_0 (SF10) no matter what I change LORAWAN_DEFAULT_DATA_RATE.
Tx power i change by call LmHandlerSetTxPower(TX_POWER_5);
But tx power is TX_POWER_0. I know the tx power by measuring current consumption.
Best Regards,
Khoa.
2022-09-14 12:43 AM
All source should be available.
Various rules in the country tables likely limits functionality by region to meet appropriate guidelines.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.