cancel
Showing results for 
Search instead for 
Did you mean: 

RSSI on LoRa-E5 vs nucleo-WL55JC1

spa23
Associate III

Hi

i'm just sitting and messing with a few lora boards.

I find that nucleo-WL55JC1 has approx 10dbm RSSI better than seeed LoRa-E5, and that nucleo-WL55JC1 also transmits with a more powerful signal, what is your experience ??

with best regards

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

What do you mean exactly when you said the clock domain on one GPIO wasn't right? Which pin?

I see an issue in my application where the receiver appears to be desensed about 10 dB. I'm wondering if I have the same problem that you were seeing.

@DWalk.3 You're replying to a nearly two year old thread, and it doesn't seem that @spa23 has had any activity on the forum since then.


@DWalk.3 wrote:

I'm wondering if I have the same problem that you were seeing.


The problem stated was with an RF switch control pin - so, if you have an RF switch, check that its control pins are really in the state they should be in...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
DWalk.3
Associate III

I saw that after the fact. It looks like my RF pins are correct.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.