2024-04-27 2:55 PM - last edited on 2024-04-28 1:00 AM by Peter BENSCH
Hi
in data sheet of different stm32WB modules, i see that max Output Power (dBm) is +6.
Why is it 6 and not 8? I thought for europe the limit is 8?
In case I want to sell the devices IN USA, max allowed TX power is even +20dbm. Does ST have any module with +20dBm?
and one generic question: I am building a wearable measuring some medical data(EMG data). Is there any standard putting a limit on TX power? Or can I go with +6 dBm?
thx
2024-05-30 11:45 AM
Hello @MK..1
Maximum output power on the STM32WB is 6 dBm. The limitations on the Maximum TX power is limited only by the low of each country.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.