2023-08-22 2:10 PM - edited 2023-08-22 2:15 PM
저는 cubeMX와 IDE를 사용하여 PWM 신호를 생성하려고 합니다.
32MHz 내부 클럭 소스(MSI)를 사용했을 때 PWM 신호 생성에 성공했습니다.
블루투스 모듈을 사용해야 하기 때문에 클록 소스를 외부 수정으로 변경했는데 PWM이 더 이상 작동하지 않습니다.
누구든지 이것에 대한 해결책을 알고 있습니까?
Solved! Go to Solution.
2023-08-22 3:10 PM
I'm trying to generate a PWM signal using cubeMX and IDE. When using a 32 MHz internal clock source (MSI), PWM signal generation was successful. I changed the clock source to an external crystal because I need to use the bluetooth module and the PWM no longer works. Anyone know a solution to this?
Probably your clock initialization failed and it's stuck in startup and never reaches the PWM code.
2023-08-22 3:10 PM
I'm trying to generate a PWM signal using cubeMX and IDE. When using a 32 MHz internal clock source (MSI), PWM signal generation was successful. I changed the clock source to an external crystal because I need to use the bluetooth module and the PWM no longer works. Anyone know a solution to this?
Probably your clock initialization failed and it's stuck in startup and never reaches the PWM code.
2023-08-23 12:12 PM
I successfully generated PWM using an external crystal HSE source using a new project.
Now, it works very well and the generated signal is more accurate than MSI.
I cannot understand why it didn't work before.
Anyway, thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.