2023-04-13 7:47 PM
I was working with stm32h723zg uart3 pin. I was using micro usb pin with stlink for uart and It works fine but I relise I have to use 3.3V power for pwr consumption test with stlink-v3pwr so I set jp2 with no jumper, and set on jp1 which it will set internal stlink off. I know by using 3.3V will make stlink unable
so I was tring to get uart signal directly from the pin. I was using usart3, I directly connect pd9 and pd8 on stlink-v3pwr but It dosent show any message on my terminal which in 5v internal stlink works fine.
so I thought the v3pwr bridge setting was wrong and try to use v3 debug port(stdc14) I found there was external debug port in h723zg(cn5 mipi10) but the connector in h723zg has no rx tx pin in cn5 so I made the pin by soldering. I test the pin and find out pd9 and pb8 was connected with my new rx tx pin in cn5 so I also test with v3pwr debug port and h723zg cn5 external debug port but dosnt show the message.
I read the datasheet and try to solder sb5 for tset which I was not using 1.8V so I was ok to by pass the level shifter still dosnt work
I even use my pL2303 serial to usb for test still dosnt work
is there any way to use uart in 3.3V input voltage without using internal stlink?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.