2021-08-20 10:25 AM
I'm working with the NUCLEO-WL55jc1 board and I have one strange behavior. I need one output pin and I've called it Trigger.
Initially, the pin PC2 was used but I wasn't able to make it work. It had incorrect output voltages and some bounce like it was a switch.
Other pins, like LEDs on the board, worked as aspected, so I decided to change the pin with PB1, using the same software: it was working.
In order to investigate, I've used both outputs, the same software, just a set, and a reset after delay. I've connected the oscilloscope to see the output signal reported in the picture.
Tack yellow is the PB1 output (Trigger_pin), track blue is the PC2 output (Test_pin) the wrong one.
My simple code.
uint16_t Distance(void) {
uint16_t distanza = 0;
UTIL_LPM_Mode_t lpm_stat = UTIL_LPM_GetMode();
// UTIL_LPM_S
APP_LOG(TS_OFF, VLEVEL_H, "\r\n###### ========== PASSO ==========, %d\r\n", lpm_stat);
BSP_LED_On(LED_BLUE) ;
HAL_GPIO_WritePin(Trigger_GPIO_Port, Trigger_Pin, GPIO_PIN_SET);
#ifdef TEST_GPIO
HAL_GPIO_WritePin(Test_GPIO_Port, Test_Pin, GPIO_PIN_SET);
#endif
HAL_Delay(10);
BSP_LED_Off(LED_BLUE);
HAL_GPIO_WritePin(Trigger_GPIO_Port, Trigger_Pin, GPIO_PIN_RESET);
#ifdef TEST_GPIO
HAL_GPIO_WritePin(Test_GPIO_Port, Test_Pin, GPIO_PIN_RESET);
#endif
Now, PC2 doesn't seem used on the NUCLEO board it's free, so my question: I've done a mistake o there is some sort of bugs on the board?
F.
Solved! Go to Solution.
2021-08-23 2:39 AM
I'm very sorry, I've wasted your time. I've made a mistake counting the PIN on the connector in reverse and wrong order so I was looking at the wrong pin.
What's worse is that I foolishly persevered.
My apologies and thank you for the help, it helped force me to revisit the connections.
F.
2021-08-22 7:00 AM
There is activity on PC2, but I'm not able to check what is controlling it.
F.
2021-08-23 12:22 AM
PC2 is not used per the user manual or the schematic. Recheck wiring, pin/port definitions. Gotta be an answer somewhere. Examine register values.
2021-08-23 1:14 AM
Maybe PC2 is declared as open drain? and what you see is the noise of the line being left floating?
2021-08-23 2:39 AM
I'm very sorry, I've wasted your time. I've made a mistake counting the PIN on the connector in reverse and wrong order so I was looking at the wrong pin.
What's worse is that I foolishly persevered.
My apologies and thank you for the help, it helped force me to revisit the connections.
F.
2021-08-24 12:26 AM
happens to the best of us
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.