2024-03-21 6:11 AM
Hello,
is it right that STM32WB55CGU6TR is already pre-loaded with FUS v1.2.0.0?
Solved! Go to Solution.
2024-03-21 8:33 AM
Every STM32WB include the last FUS Version available the day it was made. When using the Cube Programmer, the FUS is not automatically updated, you have to follow all steps mentioned on the wiki. If your question is answered, Close the topic by selecting a best answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-21 6:51 AM
Hello @strawi03 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Not sure, it depends on the manufacturing date and the available firmware. To understand which is the version on each MCU. It will be a good idea to check the version using Cube Programmer and following this wiki.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-21 7:33 AM
Hello @STTwo-32,
thank you and thanks for the quick reply.
Check with STM32CubeProgrammer results in v1.2.0.0.
So then it is clear.
I thought the STM32CubeProgrammer might automatically upgrade the FUS to the latest version.
However, this does not appear to be the case.
Thanks and regards,
strawi03
2024-03-21 8:33 AM
Every STM32WB include the last FUS Version available the day it was made. When using the Cube Programmer, the FUS is not automatically updated, you have to follow all steps mentioned on the wiki. If your question is answered, Close the topic by selecting a best answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.