2018-09-13 11:08 AM
Hi
I received this P-Nucleo-LRWan1 kit and I want to first load the EndNode code, I am using the I-CUBE-LRWAN with AC6.
Appreciate your help..
Thanks in advance!
Silas
2018-09-15 9:22 PM
Hi
I could compile the EndNode code and flash into P-Nucleo_LRWan1 kit and run successfully.
When the code runs, I see the msgs in the vcom term. I could also see the LoRa signalin the RF spectrum analyzer for each press of "userbutton" on the Nucleo.
I am using Dragino LG01-P single channel LoRa gateway and could connect to TTN.
But at this time I am not able to receive any data on TTN.
I am also working on the second part of the application i.e. using only Rx and Tx functionality. Has anone used the setup in similar way? any help will be very much appreciated..:)
Thanks
Silas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.