2019-12-29 9:27 AM
In the linker scripts for BLE_p2pServer_ota in CubeWB1.3.0, the ld script puts the OTA_TAG at 0x08007178:
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 1k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10k
OTA_TAG (rx) : ORIGIN = 0x08007178 , LENGTH = 599k
}However, the BLE_ota example checks a COMPLETELY different address in CheckFwAppValidity:
static uint8_t CheckFwAppValidity( void )
{
uint8_t status;
uint32_t magic_keyword_address;
uint32_t last_user_flash_address;
magic_keyword_address = *(uint32_t*)(FLASH_BASE + (CFG_APP_START_SECTOR_INDEX * 0x1000 + 0x140));
last_user_flash_address = (((READ_BIT(FLASH->SFR, FLASH_SFR_SFSA) >> FLASH_SFR_SFSA_Pos) << 12) + FLASH_BASE) - 4;
if( (magic_keyword_address < FLASH_BASE) || (magic_keyword_address > last_user_flash_address) )
{In particular the line:
magic_keyword_address = *(uint32_t*)(FLASH_BASE + (CFG_APP_START_SECTOR_INDEX * 0x1000 + 0x140));Checks the value of 0x08007140 (since CFG_APP_START_SECTOR_INDEX is 7).
So when we compile OTA apps with the new linker script, the MCU never boots into the main FW and stays in the OTA firmware. How can we fix this? Should we change the linker script, or change the OTA firmware which is hardcoded to check 0x08007140?
Solved! Go to Solution.
2020-01-06 5:36 AM
Indeed!
the linker file of the BLE_p2pServer_ota application in the V1.4.0 package is attached.
The OTA tag location is not defined as a region but as a section (see bellow):
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 484k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
.ota_region 0x08007140:
{
KEEP(*(TAG_OTA_START))
. = ALIGN(4);
} >FLASH
2019-12-29 9:31 AM
Just to clarify, for a previous version of CubeWB we were using (1.1.1), the linker script for BLE_p2pServer_ota points to the correct address:
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 1k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10k
OTA_TAG (rx) : ORIGIN = 0x08007140 , LENGTH = 1k
OTA_TAG2(rx) : ORIGIN = 0x08007144 , LENGTH = 483k
}
2020-01-06 3:02 AM
These errors have been corrected on the release V1.4.0 of the CubeWB FW package.
For sure you should not modify any files of the ble-ota application.
2020-01-06 4:16 AM
As V1.4.0 is not on the website yet, just to confirm the change is with OTA_TAG like this?
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 1k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10k
OTA_TAG (rx) : ORIGIN = 0x08007140 , LENGTH = 599k
}Thanks!
2020-01-06 5:36 AM
Indeed!
the linker file of the BLE_p2pServer_ota application in the V1.4.0 package is attached.
The OTA tag location is not defined as a region but as a section (see bellow):
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 484k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
.ota_region 0x08007140:
{
KEEP(*(TAG_OTA_START))
. = ALIGN(4);
} >FLASH
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.