2024-01-09 2:11 AM
Hello ST Expert ,
I'm using the NUCLEO-WL55JC1 for my project as Gateway and End-device.
I have one Gateway and 4 end device ( based on the same baord ) , i don't made any hardware change , and I'm using the SW delivered by STMicroelectronics.
I have an issue for the distance range between the Gateway and the End device.
I'm using the same configuration in all boards ( gateway and end-devices )
- SF = 11 ; Freq = 125Khz
- 22dbi
=> The maximum range is 100 metres
So ,I changed the Antenna I had 300 meters..but it is not enough for my projects.
At least i want 1000 metres to connect all End device.
Any Suggestion please I'm very blocked
Best Regards
2025-09-18 2:52 PM
Hello everyone, I'm joining this thread because I'm experiencing some similar issues. I have 2 Nucleo WL55JC2 communicating via LoRa raw at 433MHz. I've already optimized dbm (maximum allowed), SF (7) and BW(500) but I can't still reach my 1.5/2 km target of range and consider that i have a constraint of maximum 100ms of latency. At now the range is around 600m. Do you have some suggestions or could it be the limit with the standard antenna?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.