2021-01-06 11:48 PM
Have built the (single core) LoRaWAN AT Slave example from STM32Cube_FW_WL_V1.0.0, which has been flashed to a new Nucleo STM32WL55 board (straight out of the package). No apparent problems building and flashing. Configured for AS923 region.
Running an OTAA Join command the terminal returns:
AT+JOIN=1
35s069:TX on freq 923400000 Hz at DR 2
OK
35s461:MAC txDone
40s447:RX_1 on freq 923400000 Hz at DR 2
40s523:MAC rxTimeOut
41s447:RX_2 on freq 923200000 Hz at DR 2
41s523:MAC rxTimeOut
+EVT:JOIN FAILED
Looks ok but problem is that the radio isn't transmitting at all, as checked with a spectrum analyser (which sees output from other LoRaWAN boards running that frequency band).
Could be a simple configuration problem, but everything looks ok.
Suggestions would be welcome?
Solved! Go to Solution.
2021-01-07 2:22 PM
Oh Oh!
Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.
Darn. Have just ordered the correct board.
2021-01-07 2:22 PM
Oh Oh!
Answer to this question is that I have the low frequency version of the Nucleo board!! It does transmit but output is of course very weak at around 923MHz.
Darn. Have just ordered the correct board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.