2022-05-24 12:03 AM
Hi,
I am using STM32WB5MMG MCU with the latest FUS V1.2.0 and BLE_Stack_full V1.13.1.
I have my own custom BLE application. After enabling BLE fast advertisement using the API "Adv_Request(APP_BLE_FAST_ADV);", I cannot able to see the advertisement in ST BLE ToolBox Mobile App.
I am getting "BLE_STATUS_SUCCESS" as a return value.
Here I am attaching the code snippet
void Adv_Request(APP_BLE_ConnStatus_t New_Status)
{
tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
uint16_t Min_Inter, Max_Inter;
if (New_Status == APP_BLE_FAST_ADV)
{
Min_Inter = AdvIntervalMin;
Max_Inter = AdvIntervalMax;
}
else
{
Min_Inter = CFG_LP_CONN_ADV_INTERVAL_MIN;
Max_Inter = CFG_LP_CONN_ADV_INTERVAL_MAX;
}
// Stop the timer, it will be restarted for a new shot */
/* Commented out to prevent the adv from ever stopping LP 04_24_2020 */
//HW_TS_Stop(BleApplicationContext.Advertising_mgr_timer_Id);
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("First index in %d state \n",
BleApplicationContext.Device_Connection_Status);
#endif
if ((New_Status == APP_BLE_LP_ADV)
&& ((BleApplicationContext.Device_Connection_Status == APP_BLE_FAST_ADV)
|| (BleApplicationContext.Device_Connection_Status == APP_BLE_LP_ADV)))
{
/* stop any current advertising */
ret = aci_gap_set_non_discoverable();
if (ret == BLE_STATUS_SUCCESS)
{
DmConsolePrintf("BLE: Successfully Stopped Advertising \r");
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("Successfully Stopped Advertising\n");
#endif
}
else
{
DmConsolePrintf("BLE: Stop Advertising Failed | result: %d \n\r", ret);
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("Stop Advertising Failed , result: %d \n", ret);
#endif
}
}
BleApplicationContext.Device_Connection_Status = New_Status;
/* Start Fast or Low Power Advertising */
/* start the advertising */
/* modified to not sent the local name and send the adv uuid */
/* adv type changed to ADV_SCAN_IND to respond to scans LP 11-21-2019 */
ret = aci_gap_set_discoverable(
ADV_IND,
Min_Inter,
Max_Inter,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
0,
NULL,
sizeof(advertisement_uuid),
advertisement_uuid,
0,
0);
/* Update the advertising data with the manf specific data */
ret = aci_gap_update_adv_data(sizeof(manuf_data), (uint8_t*) manuf_data);
if (ret == BLE_STATUS_SUCCESS)
{
if (New_Status == APP_BLE_FAST_ADV)
{
DmConsolePrintf("BLE: Successfully Start Fast Advertising \n\r");
APP_DBG_MSG("Successfully Start Fast Advertising\n" );
/* Start Timer to get the timeout for advertising stop */
/* Commented out to prevent the adv from ever stopping LP 04_24_2020 */
// HW_TS_Start(BleApplicationContext.Advertising_mgr_timer_Id, INITIAL_ADV_TIMEOUT);
}
else
{
DmConsolePrintf("BLE: Successfully Start Low Power Advertising \n\r");
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("Successfully Start Low Power Advertising\n");
#endif
}
}
else
{
if (New_Status == APP_BLE_FAST_ADV)
{
DmConsolePrintf("BLE: Start Fast Advertising Failed | result: %d \n\r", ret);
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("Start Fast Advertising Failed , result: %d \n", ret);
#endif
}
else
{
DmConsolePrintf("BLE: Start Low Power Advertising Failed | result: %d \n\r", ret);
#if(CFG_DEBUG_APP_TRACE != 0)
APP_DBG_MSG("Start Low Power Advertising Failed , result: %d \n", ret);
#endif
}
}
return;
}
/*where as
uint8_t advertisement_uuid[] = { ZUM_ADV_UUID_ARRAY };
#define ZUM_ADV_UUID 0x75,0x63,0x9f,0x14,0xd1,0x3b,0x83,0xb2,0xb4,0x47,0xbb,0x87,0xd0,0x0e,0xA3,0x79
#define ZUM_ADV_UUID_ARRAY AD_TYPE_128_BIT_SERV_UUID_CMPLT_LIST, ZUM_ADV_UUID */
2022-05-24 1:51 AM
"I cannot able to see the advertisement in ST BLE ToolBox Mobile App"
Can you see it in any other BLE scanner apps?
2022-05-24 1:57 AM
Hi Andrew,
Even with the other scanner apps also I cannot able to see it.
2022-05-24 6:26 AM
Did you tried lightblue ble?
2022-05-25 2:49 AM
Hi Javier,
Even I tried lightblue ble app, but not able to see advertisement
2022-05-27 8:09 AM
Hello,
When you say "I am getting "BLE_STATUS_SUCCESS" as a return value." , you have check the return value of aci_gap_set_discoverable command ?
Best Regards
2022-05-29 8:42 PM
Hi,
I checked the return value of both "aci_gap_set_discoverable" and "aci_gap_update_adv_data". Both of them are giving "BLE_STATUS_SUCCESS" as a return value.
2022-06-01 2:19 AM
Hello,
If you take an application available in STM32CubeWB package, are you able to see advertising data ? For example, you can try with BLE_p2pServer example.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.