2022-03-04 5:47 AM
Hello everybody,
I'm using the AT code modified in order to join my own server with an OTAA configuration in a solar application, so every morning the system goes up, and late afternoon the system shuts down.
I want to store session keys, counters and all stuff necesary for not rejoining server each time a power down/up is done.
CONTEXT_MANAGEMENT_ENABLED is defined to 1, and I needed to add some libraries related to nvm (NvmDataMgmt.c/.h and nvmm.c/.h).
When firmware enters in LmHandlerConfigure(), I receive a "Restored", showing that we are here:
// Restore data if required
nbNvmData = NvmDataMgmtRestore( );
// Try to restore from NVM and query the mac if possible.
if( nbNvmData > 0 )
{
MW_LOG(TS_OFF, VLEVEL_M, "###### RESTORED\r\n");
CtxRestoreDone = true;
}
else
{
MW_LOG(TS_OFF, VLEVEL_M, "###### NOT RESTORED\r\n");
CtxRestoreDone = false;
}However, I try to send a message without doing a AT_JOIN and always returns AT_BUSY.
Need to send some special AT command before start sending messages? Or maybe the keys are not restored correctly?
Thank you very much!
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.