2025-08-28 7:58 AM
MCU: STM32WL55JC1
FW Version: STM32Cube_FW_WL_V1.3.1
Reference: LoRaWAN_End_Node_DualCore
Compiler/Debugger: STM32CubeIDE
Issue:
I am trying to expand the flash memory region for the CM4 application by reducing the flash memory region of the CM0+ application. When trying to modify `STM32CubeIDE/CM0PLUS/STM32WL55JCIX_FLASH.ld`:
From:
FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 120KTo:
FLASH (rx) : ORIGIN = 0x0802A000, LENGTH = 80KThe CM0+ core will never synchronize and the applications on both cores are unable to proceed. The CM4 core boots fine, but hangs waiting for the CM0+ core. If I only reduce the LENGTH of the CM0+ core it proceeds without issue.
I have also tried to modify `Common/System/system_stm32wlxx.c` by defining USER_VECT_TAB_ADDRESS and adjusting the VECT_TAB_OFFSET with no success.
What is the correct way to modify the flash allocations?
2025-09-24 6:50 AM
Hello @dbdev
Could you please give more details about the changes you maid to have this issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-24 7:37 AM
CPU2 boots according to the setting of SBRV (along with C2OPT) in FLASH->SRRVR [Ref RM0453 rev 3: Sec 2.3 and 4.10.20]. Out of the box, SBRV=0x8000 (and C2OPT=1), so it will boot from 0x08020000, which won't have the reset vector after you change the ORIGIN.
If you're not running in Secure mode (and you haven't changed C2BOOT_LOCK=0) I expect you can just write a different value into SRRVR:SBRV and then boot CPU2. [I haven't tried it.]
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.