2026-03-25 7:14 AM
Hi,
I encountered this bug with a previous update and after searching I added the -z noexecstack parameter as given in a 2025 post.
That cleared the problem at the time.
The IDE has updated itself to V2.1.1 and the bug has re-appeared, despite the noexecstack parameter still being present?
Full error:
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/thumb/v7e-m+dp/hard/crtn.o: missing .note.GNU-stack section implies executable stack
C:/ST/STM32CubeIDE_1.19.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.14.3.rel1.win32_1.0.100.202602081740/tools/bin/../lib/gcc/arm-none-eabi/14.3.1/../../../../arm-none-eabi/bin/ld.exe: NOTE: This behaviour is deprecated and will be removed in a future version of the linker(The IDE has been updated each time it prompted since the 1.19.0 install).
A second compile with no changes after clearing the error message completes OK, but this rather tedious when working on and debugging a big project.
Any work-around appreciated.
Solved! Go to Solution.
2026-03-27 7:05 AM
Hello @rjenkinsgb
Let me thank you for your feedback.
This is a known limitation marked on STM32CubeIDE:STM32CubeIDE errata 2.1.x - stm32mcu.
As work around, I recommend that you add this flag -z noexecstack under (Project > Properties > C/C++ Build > Settings > MCU/MPU GCC Linker > Miscellaneous > Other Flags) and the build will be finished with 0 errors.
[See Attachment]
Thanks
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-27 7:05 AM
Hello @rjenkinsgb
Let me thank you for your feedback.
This is a known limitation marked on STM32CubeIDE:STM32CubeIDE errata 2.1.x - stm32mcu.
As work around, I recommend that you add this flag -z noexecstack under (Project > Properties > C/C++ Build > Settings > MCU/MPU GCC Linker > Miscellaneous > Other Flags) and the build will be finished with 0 errors.
[See Attachment]
Thanks
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-27 7:56 AM
Hi Mahmoud,
thanks for the reply.
I had previously added that flag, which is why I was confused that the error was still occurring.
What I did not notice until re-checking just now is that the flag settings are separate between debug and release builds, and I had only added it in one rather than both. so it re-appeared when I changed the build I was using.
I now have it set in both which will hopefully fix the problem for good!
Thanks again, Robert.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.