2021-12-10 10:33 PM
Hello! I'm following the example here but with RF enabled to put my STM32WB into low power run mode (https://github.com/STMicroelectronics/STM32CubeWB/blob/master/Projects/NUCLEO-WB15CC/Examples/PWR/PWR_LPRUN/Src/main.c)
I'm running into an issue where whenever I call: SystemClock_Decrease(), I'm instantly losing RF connection.
Here is my system clock configuration:
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
|RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
/** Initializes the peripherals clocks
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RFWAKEUP|RCC_PERIPHCLK_RTC
|RCC_PERIPHCLK_I2C1|RCC_PERIPHCLK_RNG
|RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_HSI;
PeriphClkInitStruct.RngClockSelection = RCC_RNGCLKSOURCE_LSE;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_SYSCLK;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
PeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_HSE_DIV1024;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}I don't quite know if it has to do with the fact I use the HSE for the RF wakeup in my clock config. Whenever I select LSE, RF doesn't transmit.
Thank you!
2022-03-24 9:55 AM
Hello,
When you are in low power run mode is not supported to keep RF Subsystem enable.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.