2024-02-04 7:50 AM
Hello, I'm configuring an STM32WB55CEU6 in STM32CubeIDE and am setting up the BLE part now and I noticed that the IDE only let's me setup 5 characteristics per service. In my application (a remote control) I need about 15 characteristics. Is there a way to increase that number?
Solved! Go to Solution.
2024-02-05 3:41 AM - edited 2024-02-05 5:39 AM
Hi Nollstead,
With STM32WB, it is not possible to add more than 5 characteristics per service using STM32CubeMX. The solution would be to add the other characteristic manually without using STM32CubeMX.
This limitation has been improved on STM32WBA, with a maximum of 25 characteristics per service.
BR, Joé
2024-02-05 3:41 AM - edited 2024-02-05 5:39 AM
Hi Nollstead,
With STM32WB, it is not possible to add more than 5 characteristics per service using STM32CubeMX. The solution would be to add the other characteristic manually without using STM32CubeMX.
This limitation has been improved on STM32WBA, with a maximum of 25 characteristics per service.
BR, Joé
2024-02-05 5:35 AM
Thank you for your answer, I suspected that was the case and this explains why I saw references to 25 in a few places. Right now since I'm an STM32 newbie I'd like to stick to STM32CubeIDE so it'd probably work to spread those across three services so I'll try that.
2024-02-05 5:42 AM
Yes, it would seem to be a good solution to keep your project compatible with the Cube ecosystem.
BR, Joé
2025-03-05 2:22 PM
Would adding them manually be making calls to aci_gatt_add_char ?
It ends up with an out-of-memory error 0x98 and changing CFG_BLE_NUM_GATT_ATTRIBUTES does not seem to help. Obviously I need to learn how to do this, what resources are available?
2025-03-05 2:38 PM
For future viewers: aci_gatt_add_service() has a parameter which defines space for attributes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.