2018-12-13 7:01 AM
We use B-L072Z-LRWAN1 (Murata TypeABZ) dev board, where we were able to set-up clock sources to use HSI (@32MHz with PLL - HW_SetHSEasSysClock(void)) instead of HSE during Sigfox transmission. From the firmware perspective, everything is fine, but we were unable to receive data (Sigfox infrastructure), while the same HW with HSE is OK.
As the sigfox stack is closed, we don't know if we can do more...
What is the reason behind HSE usage? Is it the hard-requirement, or not? Is it possible to set-up HSI somehow?
Solved! Go to Solution.
2019-03-14 7:59 AM
STM's support answer to our question above was:
2019-03-14 7:59 AM
STM's support answer to our question above was:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.