2021-06-28 7:46 AM
I'm currently using I Nucleo lrwan1 shield and STM32L073 to create a Lora end node. I downloaded the latest I cube lrwan (v2.0.0) and there is no configuration to the I Nucleo lrwan1. So I can't make it work.
So, is there anyone who has the same problem or can anyone guide me to make it work.
I also posted the problem on the TTN forum and they recommended me to ask the st community about this problem
here is the link : https://www.thethingsnetwork.org/forum/t/i-cube-lrwan-problem/48864/3
2021-06-29 1:45 PM
Thanks, I'll try to find a solution and Ill post it here
2021-07-02 6:49 AM
@Community member : "Not sure ST provides firmware for the USI model"
They don't provide firmware for the USI module itself, but they do provide the AT_Master project to communicate with the USI module when it's mounted on a Nucleo board.
Unfortunately, they appear to have broken it in I-CUBE-LRWAN v2.0.0 (March 2021) :
@Imen DAHMEN - any chance of getting anyone at ST to look into this?
PS
@Imen DAHMEN - or, at least, provide a download link for v1.3.1 in the meantime ...
2021-07-02 7:07 AM
Hello,
I will try to contact expert internally to review this post.
Imen
2021-07-02 7:54 AM
https://drive.google.com/file/d/1Y141OfbyeC7fU71ZG7caRJ_xn7j1oe25/view?usp=sharing
The older versions used to present, I do have this stuff archived
There were some other reports of the support of the USI being an issue, and generally that LRWAN2 and LRWAN3 could do with some actual ownership/responsibility rather than being delivered pre-abandoned..
On another front I did port V1.1.1 to an STM32F103 platform, ~900 MHz LoRaP2P with supposedly a 2W PA driven via an 8-bit I2C DAC, toasty..
2021-07-02 9:36 AM
Thanks for the Zip.
"There were some other reports of the support of the USI being an issue"
Indeed - my name would be on some of them. It took ages to get them just to publish the schematics of the I-NUCLEO-LRWAN1 board.
:\
"and generally that LRWAN2 and LRWAN3 could do with some actual ownership/responsibility rather than being delivered pre-abandoned.."
Likewise.
ST tout these as "Partner" companies & products - there really needs to be some better commitment from both ST and these "Partners" to provide and maintain a decent level of documentation.
Perhaps @Imen DAHMEN could also find someone to look into that ... ?
2021-07-13 3:55 AM
thanks - ST expert has responded in this thread:
It is confirmed that the AT_Master project in I-CUBE-LRWAN v2.0.0 (March 2021) does not work out-of-the-box.
2021-07-13 4:04 AM
You are welcome.
Thank you for your contribution and thank you for your patience while we work on this.
Imen
2021-07-13 4:18 AM
@Community member "there is no configuration to the I Nucleo lrwan1"
Not quite sure what you mean by that?
2021-07-13 4:51 AM
@Andrew Neil as you can see here : https://github.com/USIWP1Module/USI_I-NUCLEO-LRWAN1 there are some configurations to be done depending on the I cube lrwan version.
2021-07-14 12:56 AM
Hmm ... I thought I'd replied to that yesterday?
That page refers to a very old version of I-CUBE-LRWAN - I just followed the instructions in the P-NUCLEO-LRWAN2 User Manual.
But it has been noted that these need updating for v2.0.0 of the I-CUBE-LRWAN:
>:(
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.