2021-11-05 3:57 AM
I have no problem to flash or debug the CM4 of the board. But when I'm trying to flash the CM0+ this error occurred :
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (255) Unknown. Please check power and cabling to target.
This informations are show on the consol :
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target unknown error 19
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
Solved! Go to Solution.
2022-05-13 2:30 AM
Hello @Community member ,
No problem. Unfortunately this won't be fix in V1.9 but it would be fix in the next release of the STM32Cube IDE. In the meantime please use V1.8 for dual core debugging.
Best regards
(If the previous message answer your question, please select it as Best Answer to help other customers, thank you)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.