2022-01-30 3:25 PM
I have STM32WB55RG-Nucleo board and STM32WB55CG Dongle. Current i am working on BLE_MeshLightingProvisioner project. this project doesn't have .ioc file to select the different microcontroller and i want run same BLE_MeshLightingProvisioner project in dongle.
Please help me out to select different micro-controller or share the documents for selection of different microcontroller in currant project.
Best Regards
Deepak
2022-01-31 7:13 AM
In general, assess the differences between the chips and change the necessary function. In this case, the only difference I can see is the pinout, so no code changes are necessary unless the pinout is different. In particular, the FLASH and RAM sizes are the same.
2022-02-02 3:24 AM
How about startup_stm32wb55xx_cm4.s file..?
2022-02-02 10:00 AM
What about it?
2022-02-05 7:41 AM
**Ignore the previous comment... Please consider below changes...
Here i replace the stm32wbxx_nucleo.h with stm32wbxx_usb_dongle.h (.c file also) following error i receive :
In file included from C:/Workspace STM BLE LPN Board/BLE_MeshLightingProvisioner/Middlewares/ST/STM32_WPAN/ble/mesh/Src/serial_if.c:24,
from C:/Workspace STM BLE LPN Board/BLE_MeshLightingProvisioner/Middlewares/ST/STM32_WPAN/ble/mesh/Src/mesh_cfg.c:45:
../../STM32_WPAN/app/hal_common.h:25:108: error: operator '||' has no right operand
25 | #if defined(NUCLEO_L152RE) || defined(USE_STM32WBXX_NUCLEO) || USE_STM32WBXX_USB_DONGLE /* NUCLEO_L152RE */
| ^
../../STM32_WPAN/app/hal_common.h:31:2: error: #error "Unsupported board"
31 | #error "Unsupported board"
| ^~~~~
In file included from C:/Workspace STM BLE LPN Board/BLE_MeshLightingProvisioner/Middlewares/ST/STM32_WPAN/ble/mesh/Src/serial_if.c:24,
from C:/Workspace STM BLE LPN Board/BLE_MeshLightingProvisioner/Middlewares/ST/STM32_WPAN/ble/mesh/Src/mesh_cfg.c:45:
../../STM32_WPAN/app/hal_common.h:44:1: error: unknown type name 'BUTTON_STATE'
44 | BUTTON_STATE GetButtonState(void);
| ^~~~~~~~~~~~
../../STM32_WPAN/app/hal_common.h:45:1: error: unknown type name 'BUTTON_STATE'
45 | BUTTON_STATE GetButton2State(void);
| ^~~~~~~~~~~~
make: *** [Middlewares/STM32_WPAN/ble/blesvc/subdir.mk:74: Middlewares/STM32_WPAN/ble/blesvc/mesh_cfg.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j8 all" terminated with exit code 2. Build might be incomplete.
Best Regards
Deepak Aagri
2022-03-15 6:46 AM
Hello,
For BLE_MeshLightingProvisioner project, you need an interface to send commands, so that why the project is only on STM32WB55RG-Nucleo board and not on STM32WB55CG Dongle. The following wiki page talk about this project:
https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_MESH_Embedded_Provisioning
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.