2025-05-03 9:22 PM
I can not get any output on PB9 after setting TIM16_Init:
void MX_TIM16_Init(void)
{
/* USER CODE BEGIN TIM16_Init 0 */
/* USER CODE END TIM16_Init 0 */
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM16_Init 1 */
/* USER CODE END TIM16_Init 1 */
htim16.Instance = TIM16;
htim16.Init.Prescaler = 32000;
htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
htim16.Init.Period = 65535;
htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim16.Init.RepetitionCounter = 0;
htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; // TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim16) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim16) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TIMING;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_OC_ConfigChannel(&htim16, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim16, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM16_Init 2 */
/* USER CODE END TIM16_Init 2 */
HAL_TIM_Base_MspInit(&htim16);
}and TIM17_Init;
void MX_TIM17_Init(void)
{
/* USER CODE BEGIN TIM17_Init 0 */
/* USER CODE END TIM17_Init 0 */
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM17_Init 1 */
/* USER CODE END TIM17_Init 1 */
htim17.Instance = TIM17;
htim17.Init.Prescaler = 0; //38 khz
htim17.Init.CounterMode = TIM_COUNTERMODE_UP;
htim17.Init.Period = 1725; //65535; // 1khz at 64Mhz 1msec // 63 - 1us// 1725 -38khz
htim17.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim17.Init.RepetitionCounter = 0;
htim17.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim17) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OC_Init(&htim17) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_TIMING;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_OC_ConfigChannel(&htim17, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim17, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM17_Init 2 */
/* USER CODE END TIM17_Init 2 */
HAL_TIM_Base_MspInit(&htim17);
}and MX_GPIO_Init:
GPIO_InitStruct.Pin = GPIO_PIN_9; // IR transmitter PB9
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF8_IR;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);Using the follow code in main:
__HAL_RCC_TIM16_CLK_ENABLE();
__HAL_RCC_TIM17_CLK_ENABLE();
__HAL_TIM_ENABLE(&htim17);
HAL_TIM_Base_Start(&htim17);
HAL_TIM_PWM_Start(&htim17, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 1000); // duty cycle
__HAL_TIM_ENABLE(&htim16);
HAL_TIM_Base_Start(&htim16);
HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1);What else should I try? Thanks.
2025-05-04 3:42 AM
htim16.Init.Prescaler = 32000; htim16.Init.CounterMode = TIM_COUNTERMODE_UP; htim16.Init.Period = 65535;
this sets the modulation "frequency" to the range of 0.01Hz (i.e. period around a minute). Is this what you intend?
JW
2025-05-04 8:27 AM
Yes, I would like to see any changes on PB9 using voltmeter.
2025-05-05 1:27 AM
And did you wait *minutes* to observe the change?
JW
2025-05-05 5:58 PM
Thanks, I have try many options - including - htim16.Init.Prescaler = 1000; - 1 sec.
Same voltage - 2.378 V from __HAL_RCC_TIM16_CLK_ENABLE();
to HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1);
2025-05-06 4:46 AM
I don't know then, sorry.
JW
2025-05-22 9:01 AM
Hello @GS2
I suggest you review the implementation on the X-Cube-IRREMOTE and try to adapt the examples to the STM32WB. It should be easy to migrate specially with the help of the AN4834.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.