STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Request for Hardware RF design guide for STM32WL

Dear ST Support Team,I hope this message finds you well.I am currently working on a custom RF design using the STM32WLE5CCU6 in UFQFPN48 package, and I intend to operate in the 433 MHz ISM band with +22 dBm output power.While referring to Application...

5.PNG

How to setup TIM16 and TIM17 for IR transmitter on PB9

I can not get any output on PB9 after setting TIM16_Init:void MX_TIM16_Init(void) { /* USER CODE BEGIN TIM16_Init 0 */ /* USER CODE END TIM16_Init 0 */ TIM_OC_InitTypeDef sConfigOC = {0}; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig...

GS2 by Senior II
  • 2379 Views
  • 6 replies
  • 0 kudos

P-Nucleo WB55 USB Dongle Thread Stack not working

I was able to flash the BLE full extended and run the Ble Transparent Mode in the dongle correctly. But when I want to use the Thread Cli Cmd application it simply won't work. I flash the correct stack (thread ftd bin v1.22.0 (at 0x0808B000 as the Re...

OrnellaBenzi_0-1745592752584.png OrnellaBenzi_0-1745593066590.png

UWB Module

I found this module B-UWB-MEK1 but seems like it cannot be purchased. Are there any chances that it will be released soon? Are there any alternatives for UWB position tracking? Or wireless position tracking in general?Thanks for help.

NMO by Associate
  • 957 Views
  • 2 replies
  • 1 kudos

Resolved! Data transfer via BLE to mobile app

I'm working on sensor data transfer via BLE to mobile app (like nrf connect). My STM32WB board gets connected with the app, but the data is not transmitted. When I give functions in the main while loop for transmitting, it stop the device advertiseme...

STM32WL55 & SubGHz_Phy_PingPong - UART Communication

Hi,I had an issue with UART communication in the SubGHz_Phy_PingPong middleware. The problem is that I can't receive any characters and the callback function never gets called to read the incoming bytes. Also, I figured it out from the ISR routine ev...

SiaTP by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.