2023-06-20 3:13 AM - edited 2023-06-20 7:22 AM
Hello,
I need to output an analog audio signal from STM32WB5MMGH6. I did not see any DAC on this chip so my questions are:
Is there another peripheral which can do this job that I didn't find in the datasheet ?
Also, if I can't do it with a dedicated peripheral, can you confirm that a codec is the device I need as interface?
Another solution?
Thanks
Julien
2023-06-20 3:54 AM
if you dont need top audio quality, the "standard" way is to use a timer->pwm + R_C lowpass filter, to generate analog signal.
for "hi-fi " you need a audio dac, like a PCM5102a . + connect with SAI .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.