NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I have a problem updating the Wireless Stack on STM32WB55CGU6 on a custom board. The board is basically a cloned version of the P-NUCLEO-WB55-USBDONGLE. The device is connected via SWD on St-Link/V2.FUS Version is already on v1.2 from Factory, ...
The ADS_DRDY signal (data ready signal) can be judged by the external edge interrupt method(HAL_GPIO_EXTI_CALLBACK) and reading the state of this pin(HAL_GPIO_ReadPin(ADS_DRDY_GPIO_Port, ADS_DRDY_Pin)).For the second readpin method, how should I writ...
HiI am new here using STM32WB55. I am writing drivers and API for GPIO and interrupt. But I'm facing some difficulty to find the pin for SYCFG to enable clock in APB2ENR. SYCFG is connected to the APB2 bus and when I use APB2ENR to enable SYCFG clock...
i need transfer data from node to gateway where data is taken from peer to peer from another node what i should do for that ?
I just change from gpio_raising_it to gpio falling_it(PC11). When I use raising edge interruption, all is well. When I use falling edge interruption, my led still can toggle, just can't find ble device. So I think my board can work, it's just a blue...
Hi,My problem is that I have "no stm32 traget found" message when I try to connect to a board by SWD through a ST-Link/v2 (no board identified). On oscilloscope, when we look on SWDIO pin, a little event happens when initializing connection on stm32c...
I used STM32WB55RGV6 to make a board (BLE server), the USB dongle is used as (BLE client), and then the USB dongle is output to the computer through the serial port. I need to further organize and categorize this data, and then display it as a real-t...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.