2023-05-12 3:41 PM
Hello,
I have a STM32WLE that works with the lora end_node project
I have a sensor that i power up with a mosfet when needed.
But during the time that the chip is sleeping i need to disable the internal I2C pullup (+30 uA more due to the fact that the VCC of the sensor don't control the internal pullup).
Can someone help me
Thanks
2023-05-12 4:07 PM
Write zeros to appropriate bitfields in GPIOx_PUPDR to switch off internal pullups.
JW
2023-05-28 9:49 AM
I tried it like this but error when reading i2c sensor :
void setPullUp(GPIO_TypeDef* GPIOx, uint32_t pin, uint32_t state) {
MODIFY_REG(GPIOx->PUPDR, (GPIO_PUPDR_PUPD0 << (pin * 2)), (state << (pin * 2)));
}-----------------------------------------------
LmHandlerErrorStatus_t status = LORAMAC_HANDLER_ERROR;
UTIL_TIMER_Time_t nextTxIn = 0;
MX_SPI1_Init();
MX_I2C2_Init();
MX_ADC_Init();
if(Test_SCT31()==1){
APP_LOG(TS_ON, VLEVEL_L, "Error reading id SCT31 \r\n");
Error_Handler();
}
setPullUp(GPIOA,GPIO_PIN_11,0);
setPullUp(GPIOA,GPIO_PIN_12,0);Any idea ?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.