2021-07-15 5:09 PM
I'm developing LoRa's ENDNODE using the "ENDNODE" example.
In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.
For UART setup
To change to UART2->LPUART
extern UART_HandleTypeDef hlpuart1;
I'm developing LoRa's ENDNODE using the "ENDNODE" example.
In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.
For UART setup
extern UART_HandleTypeDef hlpuart1;
I'm developing LoRa's ENDNODE using the "ENDNODE" example.
In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.
For UART setup
To change to UART2->LPUART
extern UART_HandleTypeDef hlpuart1;
I'm developing LoRa's ENDNODE using the "ENDNODE" example.
In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.
In main.h for UART setup
extern UART_HandleTypeDef hlpuart1;
#define UartHandle hlpuart1
Declared that
At uart_if.c
UTIL_ADV_TRACE_Status_t vcom_Init(void (*cb)(void *))
void MX_LPUART1_Init(void)
You have also added an msp function.
Add a function
stm32l0xx_it.c에 "void LPUART1_IRQHandler(void)"
I also added a handler.
However, neither the applog function nor the appprint function works, nor does the handler work.
Please advise which part I should revise further.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.