2022-10-03 8:41 AM
Hi!
I have a custom board built around an STM32WLE5CCU7.
My problem is that it consumes way to much power (100 times expected).
110uA in Shutdown and Standby
190uA in STOP2 WFI.
CubeMX power tool estimates these two modes to at most 0.640uA and 1.3uA respectively.
I have created a completely blank project (see attached files) which does nothing but enter various sleep-modes. It is using this project I measure the figures mentioned.
It is of course possible that I have leakage currents on my custom board, but
The board has a SMPS for generating 3v3 but I measure the current on the 3v3 after the SMPS so I dont think it should matter...
The current-diference between stop2 and shutdown is very puzzling to me, and indicates that I have (atleast one) software issues.
I'm at a complete loss here and very grateful for any suggestions on how to proceed the fault finding..
Edit: I have the debugger physically disconnected during measurements (and powercycle the chip after disconnectintg the debugger)
Best Regards
Axel
Solved! Go to Solution.
2022-10-19 1:25 AM
Hello @AAlat.1 ,
Have you try the PWR_STANDBY single core example provide in the FW package STM32Cube_FW_WL_V1.2.0 ?
This could help you to determine if this come from your software or if you still have an issue with your hardware.
Also you can find here an article from a member of the community that explain how to enter in standby.
I hope this help you, let me know if you succeed.
Best regards
Louis
2022-10-19 1:25 AM
Hello @AAlat.1 ,
Have you try the PWR_STANDBY single core example provide in the FW package STM32Cube_FW_WL_V1.2.0 ?
This could help you to determine if this come from your software or if you still have an issue with your hardware.
Also you can find here an article from a member of the community that explain how to enter in standby.
I hope this help you, let me know if you succeed.
Best regards
Louis
2022-11-01 1:14 PM
Thanks for your reply, and sorry for my late response!
I keept comparing my code to your links and eventually found the issue.
The issue itself was twoffold.
Problem 1
Was hardware, the RF-switch (taken from the reference design) seems to consume 110uA. We had missed that during schematic check :unamused_face:. After desoldering the switch shutdown mode consumed <2uA (Cannot measure more precise in my current setup)
Problem 2:
STOP2 mode issue remained and consumed 80uA. I erroneously thought all pins were analog-input by default (which some parts of HRM can lead you to believe). It seems the debugger pins (PB3-4, PA13-15) are exceptions that are configured in peripheral mode (which thinking about it makes sense, otherwise the debugger cant control a blank chip after reset).
After manually setting these 5 pins to analog input stop2 also consumes <2uA.
My problem is solved for now.
Now I need to turn things on one at a time and see that I can retain the low power in sleep, but now I have a baseline to work from!
2023-11-15 7:57 PM
Sorry...I am Vietnamese
Can you give me your <2uA sample project... when I use it, it is at 290uA
i tried a lot of different ways but couldn't get it down to even <10uA
2023-11-15 11:06 PM
sorry.....I don't know where to ask, so I have to ask here
i can't sleep at <10uA, i'm using RAK3172 with arduino firmware then i can sleep at <10uA when i use cubemx i can't deep sleep specifically at 290uA
2023-11-16 12:13 AM
Hello @AD1 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
It will be better if you create a new Post on the STM32 MCUs wireless Forum and give more details about your problem.
Best Regards.
STTwo-32
B
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-16 12:39 AM
I can't post because I'm new to this... is there any way to help me get back to deep sleep as quickly as possible?
2023-11-16 12:49 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.