2019-05-04 8:34 AM
The answer from the processor is
RSS state is WIRELESS_STACK_UPGRADE_ONGOING
RSS status is RSS_IMAGE_NOT_FOUND
RSS state is RSS_IDLE
RSS status is RSS_NO_ERROR
Firmware Upgrade process started ...
Updating firmware ...
Firmware update finished
Firmware Upgrade command execution finished
I tryed with all the software (server, client ecc.) but it doesn't work.
What I do not understand is that in help description it is said that file name and address are optional in fwupgrade command. How is it possible ? If I do not specify the binary file with the stack, how can it flash inside the micro ? Maybe they are silly questions, but I do not really understand where I am wrong. Thank you very much for helping me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.