2019-07-18 12:29 AM
The mesh library for the STM32WB55 only seems to be compiled for the IAR compiler as of right now, and there also seems to be an older version of the BlueNRG mesh library available for keil. These compilers are both very expensive and do not work under linux.
Are there any plans to release a gcc version or even the source? As it is, the library is unusable for me, which is not great when the device is marketed as mesh compatible.
2019-07-18 1:20 AM
The mesh compiled library for the STM32WB55 will be available for IAR, MDK-ARM and SW4STM32 in the STM32Cube_FW_WB_V1.2.0 delivery.
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.