2024-11-10 9:56 PM
Hi Guys,
I was planning to start a project using the STM32WB55 chipset to implement a device capable of connecting to both Zigbee and BLE devices via a dynamic concurrent mode approach. I was able to confirm that this device supports it from the thread https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_Dynamic_concurrent_mode_BLE-Zigbee I'd also like to confirm if the WBA series supports this feature. Given that the WB55 is a dual-core (M4/M0+), and the WBA series is based on the M33 core, I need to verify if the WBA series can support Bluetooth Low Energy® and Zigbee dynamic concurrent mode for this project. I couldn't find anywhere specific that says it doesn't support dynamic mode and I guess WBA is a very different series compared to WB. Please share your knowledge on this.
Looking forward for your response.
Solved! Go to Solution.
2024-11-21 9:06 AM
Hello @justinjoseph
I can confirm that the Dynamic-concurrent mode Bluetooth Low Energy/Zigbee is supported by the STM32WBA. To understand how it works. You may can refer to this example: BLE_Zigbee/BLE_HeartRate_Zigbee.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-21 9:06 AM
Hello @justinjoseph
I can confirm that the Dynamic-concurrent mode Bluetooth Low Energy/Zigbee is supported by the STM32WBA. To understand how it works. You may can refer to this example: BLE_Zigbee/BLE_HeartRate_Zigbee.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.