2023-03-29 7:06 AM
I am trying to use the WL55 with a legacy 2-gfsk system that relies on CC1120 chip.
The major issue here is related to de-whitening of the received data.
I am editing the subghz ping pong example.
Band, AWG and datarate are coherent with the legacy system, but the data I receive is waaaaay too long compared to the expected (and transmitted) one.
First issue: I'd like to receive all the data over the air, preamble and sync word included. I am not sure I am receiving it because the data does not look like the sync word (that is 0xAA in the CC1120 and 0x55 on the WL55). I am relying on the variable-length packet format BTW.
Second issue: in Variable length packet format the whitening is applied both in tx and rx ALSO to the legth byte hence the data I receive is arbitrarly long.
Third issue: the PN9 algorythm in CC1120 and in WL55 are different, something related to IBM vs CCITT, hence the only solution I can figure is to receive whitened packets and de-white them in software. I don't think changing the initial seed for the algo could help me in any way.
Any hint on these 3 points?
K.R.
L.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.