cancel
Showing results for 
Search instead for 
Did you mean: 

Custom wireless stack on STM32WB55 devices

JTres.2
Associate II

Hi,

I'm looking into using the STM32WB55 device for a custom radio solution.

From what I gather this same question was asked and answered here: https://community.st.com/t5/stm32-mcus-wireless/is-it-possible-to-flash-a-custom-application-to-cpu2-m0/m-p/288448

Since the post is 4 years old I just want to make sure this is still relevant and that its not possible to make custom binaries for the M0 coprocessor due to encryption key managed by ST?

Br

Johan

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @JTres.2 

As a quick answer, yes the code expected to be executed by the CPU2 must be encrypted with specific ST key that the FUS (Firmware Update Service) is the only one to manage. 

So yes, the post still relevant.

Best R

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @JTres.2 

As a quick answer, yes the code expected to be executed by the CPU2 must be encrypted with specific ST key that the FUS (Firmware Update Service) is the only one to manage. 

So yes, the post still relevant.

Best R

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.