2022-05-18 9:30 AM
Hi,
Is there any side effects of changing the RF Frequency of the Lora Modem during runtime.
Radio.SetChannel(RF_FREQUENCY);Can this be used to change the frequency at runtime?
Thanks
2022-05-20 8:42 AM
Hello @MCarl.7 ,
If you look in the SX1261-2 specification here, you can see in the section 9.4 Standby mode, that you have to be in standby to configure your radio before going in Rx or Tx mode.
I hope it helps
Regards
2022-05-20 12:40 PM
You can change settings, usually a structure/variable.
As indicated you'd typically do so as you cycle between RX, TX, STANDBY/IDLE states in the main() loop of most of the LoRa examples/demos
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.