2021-01-04 4:05 AM
2021-01-04 7:14 AM
Hi, RBG,
the RM0434 describes the usage of the internal Flash memory. Section 3.3.8 provides useful information on the size of the data that can be written, e.g.:
The Flash memory is programmed 72 bits (a double word, 64 bits plus ECC, 8 bits) at a time.
Programming in a previously programmed double word is only allowed when programming an all 0 value. It is not allowed to program any other value in a previously programmed double word, any attempt sets PROGERR flag in the Flash memory status register (FLASH_SR) or Flash memory CPU2 status register (FLASH_C2SR), except when programming an already programmed double word with an all 0 value.
It is only possible to program a double word (2 x 32-bit data).
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
/Peter
2021-01-04 12:18 PM
Groups of them anyway...
Perhaps if you're more specific about the end goal, you'll get some better answers / suggestions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.