2021-08-21 6:14 AM
I'm trying to add an external FLASH and RAM to the STM32WB55, but he doesn't have an FMC or FSMC, and all resources a could find related to this subject use the FMC peripheral, there is any way to use the external RAM and FLASH in the same time?
should I use 1 QSPI for both of them?
Solved! Go to Solution.
2021-08-21 7:16 AM
No.
You can only use one, the design is optimized for a QSPI NOR Flash, allows for execute-in-place.
What kind of FLASH/RAM resources does your application need?
2021-08-21 7:16 AM
No.
You can only use one, the design is optimized for a QSPI NOR Flash, allows for execute-in-place.
What kind of FLASH/RAM resources does your application need?
2021-08-21 7:27 AM
hey, thank you for your reply
I'm looking for an extra 1 Mb of RAM and more than 4 Mb of flash.
what do you think is the solution?
I can optimize the flash because I will use it for a GUI product.
2021-08-21 8:42 AM
Mb bit
MB Byte
What do you need 1MB of RAM for?
Perhaps look to a display/controller with it's own on-board frame buffer memory, and which you can communicate with via SPI.
Consider pairing with another MCU with more flash, ram, and capabilities.
2021-08-21 8:51 AM
I'm already using an LCD with it one frame buffer
I want this size of RAM for future updates and the RTOS.
I don't want to update the hardware in the future.
But anyway, I will go with the available RAM in the MCU.
Thank you for the information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.