2021-09-16 8:02 AM
I'm working on the application project LoRaWAN_AT_Slave_DualCore from STM32Cube_FW_WL_V1.1.0 .
The payload of the downlink messages is not correctly transfered from the processor M0 to the processo M4.
There is a bug in:
file LmHandler_mbwrapper.c,
function static void OnRxData_mbwrapper(LmHandlerAppData_t *appData, LmHandlerRxParams_t *params):
if (appData != NULL)
{
UTIL_MEM_cpy_8(aLoraMbWrapShare2Buffer, appData, sizeof(LmHandlerAppData_t));
/* need to 8-align the next address */
next_addr = (sizeof(LmHandlerAppData_t) + 7) & ~7;
if (appData->BufferSize > 0)
{
UTIL_MEM_cpy_8(&aLoraMbWrapShare2Buffer[next_addr], appData->Buffer, appData->BufferSize);
((LmHandlerAppData_t *)aLoraMbWrapShare2Buffer)->Buffer = &aLoraMbWrapShare2Buffer[next_addr];
next_addr = (appData->BufferSize + 7) & ~7;
}
}
The bold line should be removed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.