2021-12-23 9:22 AM
Hello,
I am developing a project that includes a bootloader and an application to jump to.
Both binaries execute on the M0+ core in order to take advantage of the security features offered only for this core.
The idea is as follows:
The bootloader verifies the integrity/authenticity of the application and then jumps in it.
I am trying though to enable the hide protection (HDP) feature to allow the execution of the bootloader after a reset or power cycle and then protect the flash area where it is located.
In other words, I need the bootloader to be in a secure area and protected from potential read or write actions.
Based on the RF0453 I must call the RSSLIB_PFUNC->CloseExitHDP funtion from my bootloader to close the HDP area and then jump to my application.
Without enabling the HDP I can verify that the bootloader jumps to my application by using the RSSLIB function above.
When I enable the HDP, though, it seems as if the RSSLIB_PFUNC->CloseExitHDP funtion never jumps to my application.
The bootloader is located in flash offset 0x08020000.
My application is located in flash offset 0x08001800.
So, based on that I enable the HDP as follows:
To jump to my application I call the following line in my bootloader:
RSSLIB_PFUNC->CloseExitHDP(RSSLIB_HDP_AREA1, 0x08001800);I keep trying to read any related documentation such the the reference manual but it seems as if I miss somthing.
Please, let me know if you need further information to make things more clear!
Thank you!
Solved! Go to Solution.
2022-01-10 2:11 AM
I found the solution to my problem so I share it in case it is useful to anyone:
At page 68 of RM0453 Rev 2 it states the following:
"The secure area of the memories have exclusively read, write, execute access only from the secure CPU2 and secure DMA channels"
At the same page it, also, states:
"CPU2 has only read and write access to the non-secure areas. CPU2 is prevented from executing from non-secure areas"
So, my mistake was that when I enabled the security I set as secure area the one starting from page 0x40 (0x8020000) which is the area where ONLY the secure bootloader is stored.
The application was stored in flash starting at page 0x3 (0x8001800) which is not part of the secure area, so, since security was enabled CPU2 could not jump and execute in this non-secure area.
So, what must be done to make it working is:
In this way the security is enabled and the secure flash area includes both the secure bootloader and the application.
Additionally as previously:
This enables the hide protection feature ONLY for the secure bootloader area which is executed at a device reset or device startup and then when jumping to the application this area is no longer accessible (hidden).
2022-01-10 2:11 AM
I found the solution to my problem so I share it in case it is useful to anyone:
At page 68 of RM0453 Rev 2 it states the following:
"The secure area of the memories have exclusively read, write, execute access only from the secure CPU2 and secure DMA channels"
At the same page it, also, states:
"CPU2 has only read and write access to the non-secure areas. CPU2 is prevented from executing from non-secure areas"
So, my mistake was that when I enabled the security I set as secure area the one starting from page 0x40 (0x8020000) which is the area where ONLY the secure bootloader is stored.
The application was stored in flash starting at page 0x3 (0x8001800) which is not part of the secure area, so, since security was enabled CPU2 could not jump and execute in this non-secure area.
So, what must be done to make it working is:
In this way the security is enabled and the secure flash area includes both the secure bootloader and the application.
Additionally as previously:
This enables the hide protection feature ONLY for the secure bootloader area which is executed at a device reset or device startup and then when jumping to the application this area is no longer accessible (hidden).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.