STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WBA55CG ADC DMA CIRCULAR

hello,I want to set up a timer2 TGO triggered DMA system with 60 samples in 20ms from 4 channels.I made the linked_lisit settings etc. via CubeMx but I can't get a sample from the ADC.Can you help me?

Resolved! aci_gap_adv_set_scan_resp_data returns 0x0C

Hi allwhen i try to call the function to add scan response data to my advertising data I get the error 0x0C. I get the error code means that operation is not allowed, but nowhere it tells how to call a function in order to be allowed. I am susing STM...

cvs_dev_0-1747230228710.png
cvs_dev by Associate II
  • 1199 Views
  • 1 replies
  • 0 kudos

Resolved! How to obtain the .ioc file

在 STM32Cube_FW_WB_V1.22.1\Projects\P-NUCLEO-WB55 下。Nucleo\Applications\BLE 中,某些文件有。IOC 文件,而其他文件则没有。例如,在 BLE_CableReplacement 中,没有。与 STM32CUBEMX 相关的 IOC 配置文件。如何获得?

Thorn by Associate
  • 2115 Views
  • 4 replies
  • 1 kudos

Resolved! Problem with ADC on custom board

Hello.I have a problem with the ADC on the custom board with the STM32WB55 chip. I am using a divider and should get something around 2V, but I always get the maximum value - 4095.I am using this code that I saw in the ST examples. HAL_GPIO_WritePin...

IlliaGx by Senior
  • 6526 Views
  • 19 replies
  • 12 kudos

Resolved! NUCLEO-WBA65RI BLE examples not working

I tried to run two examples on my new NUCLEO-WBA65RI. Specifically the 'BLE_p2pServer' and the 'BLE_HeartRate'. I followed this guide for the p2pServer:https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WBA_Build_BLE_ProjectBuilding works but when I...

strg-v by Associate II
  • 2799 Views
  • 7 replies
  • 0 kudos

Resolved! LoRaWAN region

I am developing an application from LoRaWAN End Node example in STM32WLE MCU that has to work in different countries. To select easily the LoRaWAN region from hardware I have dedicated three pins as GPIO Inputs. The idea behind is that by reading the...

alefarri by Associate II
  • 1279 Views
  • 2 replies
  • 1 kudos

Help with SystemClock_Config

How to combine settings in SystemClock_Config to use both keyboard and ADC examples? In keyboard project there is the follow setting in SystemClock_Config: RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MS...

GS2 by Senior II
  • 2738 Views
  • 8 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.