2025-07-14 12:22 AM
Hello,
I am working on a project using the STM32WBA microcontroller and looking for a way to provide Wi-Fi connectivity in order to connect the system to a web server.
I've read in several places across ST's website that the STM32WBA series supports OpenThread Border Router (OTBR).
However, I couldn't find clear information on whether the STM32WBA can act as a standalone OTBR, or if it's limited to acting as a Radio Co-Processor (RCP) like some examples for the STM32WB series.
Does anyone know if it's possible to use the STM32WBA alone as a full OTBR? Or would I need to connect it to an external host that handles the Wi-Fi stack?
Any clarification or pointers to official documentation would be really appreciated!
Solved! Go to Solution.
2025-07-14 12:48 AM
Hello @aboabra and welcome to the ST Community.
A OpenThread border router (OTBR) is a specific router that connects a Thread network to other IPv6-based networks like Wi-Fi or Ethernet. Since the STM32WBA does not support Wi-Fi or Ethernet connection, so it can’t be a OTBR but it will need a host for IPv6-based network.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-14 12:48 AM
Hello @aboabra and welcome to the ST Community.
A OpenThread border router (OTBR) is a specific router that connects a Thread network to other IPv6-based networks like Wi-Fi or Ethernet. Since the STM32WBA does not support Wi-Fi or Ethernet connection, so it can’t be a OTBR but it will need a host for IPv6-based network.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-14 12:50 AM
Thanks for the fast response!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.