STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

BLE Mesh & Gateway

Hi All,May i check with you all on the following question, 1. The data needs to be sent to server/cloud, therefore a gateway is required. Does ST have a solution on the BLE gateway?2. If the BLE Module is used, mesh topology will be employed. Does ST...

Pooh.T by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

Problems with ATSlave connecting to the TTN Network.

Hey thereWe are developing LoRa Applications based on I-CUBE-LRWAN Stack. 1.5 Years ago, i ported it into a freertos and it worked great. now i'm trying to port the newer version of the stack and i'm not able to connect to the things network. to my o...

Code has to be re-generated whenever I re-open the IDE

I'm using the P-NUCLEO-WB55 development board, with only USB (CDC Device) and USART1 enabled/configured through the STM IDE.The code is generated, I add my own code, I compile, program, test it, and everything works.However, whenever I close and open...

pierpaolo by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

Resolved! Stop advertising due to SCH_SetTask()

Hello everyone,I am working on a project on which i would like to send a notification from a board to another when the firts one crosses a threshold with the built-in comparator. I started from the BLE_p2pServer and BLE_p2pClient examples from STM32C...

Franklin by Associate II
  • 2872 Views
  • 6 replies
  • 0 kudos

STM32WB Dongle as central

Hi, I'd like to know how to use a STM32WB Dongle as central to interface a PC windows App to communicate with a STM32WB DK. Are there any examples I can use as a starting point?

Debugging startup won't progress past: bl SystemInit

Firstly I'm very new to all of this so apologies if this is trivial.I have been trying to debug and run a simple blinking led project onto a STM32WB nucleo board using the STM32CubeIDE v1.0 (MacOS). After staring the debugging session, the console di...

Dossy by Associate II
  • 14865 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.