NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm trying to register a P-L496G-CELL01 Discovery Kit in the Concierge portal at www.stm32-c2c.com. The problem is that the portal doesn't seem to recognise that I click the confirmation email. Each time I try to register the new board, it just asks ...
Has the API for the bluetooth, i.e. the aci_gatt_update_char_value etc etc
Hello, I am facing problems with installing the DFU Driver on my PC, I have followed the steps which are mentioned in UM2237 document which are the following: 1- installing STM32Cube Programmer 2- run STM32Bootloader.bat as administrator 3- put the N...
I follow the instructions here:https://docs.zephyrproject.org/latest/boards/arm/nucleo_wb55rg/doc/nucleowb55rg.htmlI've built the .elf file, how do I flash this to my board? I see my board connected as a drive, I copy the elf file over but when I dis...
Hi, In my application i try to use a second nucleo board as Client. In the Android App my Service is shown as temperature value.Now i have Problems with get the specific data in the nucleo Client.Is there any Tutorial or how to for register the ch...
Hello,I've just bought the STM32WB Nucleo Kit to develop an application. I've programmed with MCUs in the past mainly Arduino but also with the ATMega 168 directly. To learn how to use the STM32 I started watching this playlist from YouTube which is ...
Hi, i am trying to use this function but always return me 0uint32_t SysTime2Ms( SysTime_t sysTime ) { SysTime_t DeltaTime; HW_RTC_BKUPRead( &DeltaTime.Seconds, ( uint32_t* )&DeltaTime.SubSeconds ); SysTime_t calendarTime = SysTimeSub( sys...
I am new to Bluetooth development so maybe the answer is obvious. I would like to use BLE on a wearable for indoor localization with Eddystone beacons, so far so good. At the same time (or in a timeframe) I would like to transmit information via BLE ...
I want to switch between ZIGBEE and BLE online
Sorry for such a newbie question....I can connect and debug in CubeMX, was trying to get a project started in CubeIDE.I can select the CPU, but I don't see the board package. Is there some initialization I might be missing? IDE connects, then pausing...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.