STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

How to flash the firmware on STM32F7 wirelessly (OTA)?

Hi,Is there an existing infrastructure for OTA custom firmware flashing of an STM32F7 MCU using (preferably) STM32WB of SPWF04?we have an already written application for our STM32F7 which takes more than 512KB.I went through the resources and found o...

APilk.1 by Associate
  • 1157 Views
  • 0 replies
  • 0 kudos

Resolved! Connection problem for new board design

I designed new board with STM32WB55CGU6 based on MB1993C (P-NUCLEO-USBDongle). You can see my schematic attached(I uploaded both P-nucleo schematic and my schematic). But I can't connect to my MCU through SWD pins (DIO,CLK,NRST). I use st-link, I can...

ashkanr65 by Associate II
  • 1601 Views
  • 1 replies
  • 1 kudos

How do I get 32Mbps SPI?

I’m using the nucleo board, and I’ve got SPI working correctly (mostly) with default settings using CubeIDE. However, the data sheets stated that SPI can run at 32 Mbps, and I’m only getting half that rate.The SPI Prescaler is set to the minimum valu...

ASmit.4 by Associate II
  • 4821 Views
  • 9 replies
  • 0 kudos

STM32WB55 BLE OTA issue

Hi,I am working with OTA on STM32wb55 wireless MCU,I have tested BLE OTA from android app mentioned in AN5247 and it worked well.Now i need to create a python app doing the same.In order to do that i followed Flow given in the same AN5247 at Figure 9...

RTriv.1 by Associate II
  • 1624 Views
  • 2 replies
  • 0 kudos

the current consumption of the STM32WB55 in stop2 mode is about 116uA whici is much higher than it should be in the datasheet about 2uA.

I test it on P-NUCLEO-WB55 kit board which without any other devices connected on it with the official examples "PWR_STOP2_RTC" ,and I did test it as the readme.txt file tell me(remove all jumpers on JP5, and test the current on the JP2), but the res...

zxiao.2 by Associate II
  • 1851 Views
  • 3 replies
  • 0 kudos

I am trying to use STM32W55RG as BLE client in FREERTOS CMSIS V2. But it seems that its not allowed. May i know the reason behind this?

I am trying to use STM32W55RG as BLE client in FREERTOS CMSIS V2. But it seems that its not allowed. May i know the reason behind this? I attached the error image in this message. I also observed that Sequencer is also not available in FREERTOS. Can ...

0693W000000VjAhQAK.jpg

STM32Cube MCU Package for STM32WL series not available.

​STM32Cube MCU Package for STM32WL series (HAL and LL low level drivers, USB, File system, RTOS - coming with examples running on ST boards: STM32 Nucleo, Discovery kits and Evaluation boards) not available on st site. Please provide me mcu packages ...

Cyada.1 by Associate II
  • 1760 Views
  • 2 replies
  • 0 kudos

Running STM32CubeExpansion_LRWAN_V1.3.1 on AcSiP S76G

Hi,I tried running ST lorawan stack (STM32L073RZ-Nucleo) on acsip s76G chip (with stm32l073RZ and sx1276). I can get data from device but the problem is that the signal is too weak. I know my hardware is ok so what should i config in code? Any sugges...

IZama by Associate
  • 899 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.