NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am currently playing around with LoRaWAN and TTN and try to getting SX1276 Modem (nice RF) to work.I implemented on STM32l4 board. When OTAA join starts the device gets registered on the TTN console but i never receive the join accept back on my no...
Good Day.I want to put my stm32wb device to sleep standby mode. and wakeup using RTC after specific time.I am following the PWR_STANDBY_RTC example which works.I would like to sleep for up to 12 hours and would like to use RTC_WAKEUPCLOCK_CK_SPRE_16...
Dear Support,I'm using the SX1272 in lora mode in my application. I have both products that communicates together. They are configured in Rx single with a symbol timeout equal to 1000. When no communication the rxtimeout is about 1023ms. But when the...
Hello ST Community,Let's start with my problem:I have a STM32WB55CG chip that I want to get working in BLE. I also want it to have an USB CDC interface.I created a project on cubeMX, added my external oscillator (32MHz), activated the USB device unde...
I'm developing an application which uses both USB mass storage and BLE. I've started by building two separate applications using STM32CubeMX:A USB mass storage application communicating with a microSD card over SPI1A BLE P2P serverBoth of these work ...
I would like to be able to turn BLE off (e.g. with a timer) even if it is currently connected. I know I can stop it advertising, but this doesn't seem to kill the connection. Basically, after a timeout, I would like the BEL to shutdown and stop using...
Hello! I am using PWM to generate 1.25 ms period pulse to trigger a LED strip light . In main.c , properly in while(1) when I called HAL_TIM_PWM_Start_DMA followed by HAL_Delay the program got stuck in uint32_t tickstart = HAL_GetTick(); . When I run...
I have a custom test/debug fixture for a custom board. It is based on the ST-LINK/V3-MODS board to programm the target MCU (STM32WB55).The other interfaces (GPIO, I2C) are used to control functions like power supply to the target etc.When I try to de...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.