STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

SRM32WB55 junk data over LPUART in interrupt mode

Hello,We came across a strange problem with LPUART on STM32WB55 chip.When using FIFO in interrupt mode (receiving data), if you use FIFO depth more than 1 byte (even 2 or 8) you will occasionally (one out of ~1000 reads) get complete junk bytes (not ...

APort by Associate III
  • 2029 Views
  • 3 replies
  • 0 kudos

Creating custom bluetooth service/charasteristic

Hello. I have ordered stm32wb development board and recently started to learn about the Bluetooth. I am planning to control an electric lock through bluetooth mobile app.I have seen the stm32wb workshop, especially part 4 where they are creating a cu...

LPetr.1 by Senior II
  • 769 Views
  • 0 replies
  • 0 kudos

Receiving HCI_HARDWARE_ERROR_EVENT from BLE Stack

MCU: STM32WB55BLE: BLE Stack Full V1.8.0Hello,I am using STM's BLE OTA example project (bootloader) and have it working with my custom firmware. I have noticed an issue that happens when updating my custom firmware via ota. Every so often I am unable...

Resolved! Clipped sine TCXO for STM32WLE5

Greetings,STM32WLE5 reference manual says an external TCXO should have a sinusoidal output. Clipped sine oscillators seem to be more available, do you think they would work too?Thanks!

OYTIS by Associate
  • 2009 Views
  • 1 replies
  • 0 kudos

How to use the EEPROM emulation example code "EEPROM_Emul" from"X-CUBE-EEPROM_V2.0.0" package on a custom STM32WB55CE board.

I have my custom STM32WB55CE board. I had programmed the example code "EEPROM_Emul" from"X-CUBE-EEPROM_V2.0.0" package on it. It was working fine. Then I did FUS upgrade with BLE full stack binary programming on it. After that, the same EEPROM emulat...

GBehe by Associate III
  • 30124 Views
  • 30 replies
  • 1 kudos

Multicast messages on LoRa Murata Module (I-CUBE-LRWAN)

Hello, I ask here a question already asked in another topic and which as not received any answer.**** I would like to know how toimplement Multicast messagingon my end-node (currently using Murata Module (CMWX1ZZABZ-078) with ST LoRalibraries (Expans...

FRIGA by Associate
  • 1069 Views
  • 1 replies
  • 0 kudos

How can I explore ZigBee 3.0 in STM32WB55cc MCU's , I want to control the street Light(ON/OFF) and continuously read the state of Light.

Hello,Currently our team is working with "STM32WB55 P-NUCLEO-WB55 Platform", we were able to flash the stack.Then we have tried the same ZigBee project and able to self-demonstrate the same successfully, like led on/off and sending messages.As our te...

Csrik.1 by Associate II
  • 937 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.