STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

BLE_Beacon Example on STM32CubeIDE and P-Nucleo WB55

I'm trying to make the "BLE_Beacon" example found inside the "STM32CubeWB" file work with the STM32CubeIDE and the P-NUCLEO WB55 board. The program compiles correctly but I can't see the beacons. Debugging I saw that when it arrives in the UTIL_SEQ_R...

AAoe.1 by Associate II
  • 625 Views
  • 0 replies
  • 0 kudos

How to synchronize two RTC?

Hi I have two custom boards with stm32wb55 with a external crystal oscillator for the rtc. One device should be the master and the other is the slave. Master should set the rtc for the slave. Is it possible to sync them over ble with a precision of ...

suads by Associate III
  • 1930 Views
  • 1 replies
  • 0 kudos

STM32wb BLE disconnection callback function hci_disconnection complete event() not triggered

Stm32wb BLE callback function:  void hci_disconnection_complete_event( uint8_t Status,                    uint16_t Connection_Handle,                    uint8_t Reason ){ printf("hci_disconnection_complete_event");}not working.STM32WB use a utility f...

Aishwarya by Associate III
  • 914 Views
  • 0 replies
  • 0 kudos

SDIO and WiFi Driver for Murata Type 1MW for STM32F4

Hello,We are working on integrating Wi-Fi module Murata Type1 MW LBEE5HY1MW(Cypress CYW43455) with STM32F4 based micro-controller using SDIO interface.We are looking for SDIO Driver and Murata Wi-Fi driver for STM32F4 based micro-controller.anyone he...

DShar.3 by Associate
  • 1218 Views
  • 0 replies
  • 0 kudos

STM32WB, PA2/PC13 ERRATA clarification needed.

The ERRATA says essentially that port activity on PA2/PC13 will disturb LSE (WCLSP100)Does that mean that I can use PA2 still as LSCO ?Does that also mean that I still can use PC13 as RTC_TS / RTC_TAMP, or as WKUP2 ?Which ones will be a problem, or i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.