NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi all,I have the STM32WB55 board connected to a battery. However it loses connection (firmware does continue without issues) quite often. After some research I have found out that when i attach the charger or the st link the disconnection issue is g...
Hello!Is there an overview of how big the ST wireless stack is depending on the activated features?Thank you!
Hi,I have P-NUCLEO-LRWAN2 starter pack and I'm trying to run AT Master application on NUCLEO-LRWAN1/NUCLEO-L073RZ pair with supplied in I-CUBE-LRWAN Expansion Package. It looks like all fine (i.e firmware compiled and loaded onto NUCLEO-L073RZ withou...
I bought p-nucleo lrwan2 working with STM32LO MCU,and i'am wondering to configure its device sensor as end node ,watching the last video posted by ST they were working with the same pack but they targered STM32WL as end node instead of working with t...
This is the only code I could find. There is no information about which device this can be used with either. please help me
I want to use software uart in NUCLEO-WL55JC2.
Hi guys. When I program the device with LoRaWAN and DAC with pin extern (PA10), I saw in oscilloscope that DAC stay high every when has uplink. Like the image: Does anyone have any idea why this happens? Thanks!
Hi,I am looking for a dual core controller and options I have been able to find out are:Stm32Wb seriesStm32H seriesBeing, H series quite expensive, Is it possible to use WB series M0+ for running another application in parallel?Or we can only use it ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.